How can we help you today?

Compact ADU206/256/210 to X80 AMI0410 quick wiring - 990XSM00210

Issue

Migrating an ASBADU206/256/210 to a BMXAMI0410 and need to confirm the 990XSM00210 quick wiring cable pinout.

Product line

Modicon X80, M340, M580

Resolution

Below is an image of the pinout.

pinout

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: