How can we help you today?

HMI License Manager 2.1.1.0 Installation Wizard was interrupted

Issue

When running the HMI License Manager 2.1.1.0 installer from the Schneider Electric Software Update Tool, the following message appears:

"The Installation Wizard was interrupted before HMI License Manager could be completely installed"

Installation Wizard was interrupted message

Product Line

HMI License Manager (for Vijeo Designer 6.3 or higher and EcoStruxure Operator Terminal Expert v4.0 or higher)

Environment

Windows 10 / Windows 11 Professional

Cause

The HMI License Manager first detects if there is an older License Manager and uninstalls it, then it checks for whether or not there is an older version of the Schneider Electric Software Update Tool older than the current version (3.0.12.0 at the time of this writing). If it is older, it will proceed to upgrade it to the latest version. If the Schneider Electric Software service is running and it is currently writing to disk, it will not be able to be updated.

Resolution

To solve this issue, follow these steps:

1) Obtain the latest installer file for the Schneider Electric Software Update tool (v3.0.12) by opening this URL in your browser:

https://www.seupdate.schneider-electric.com/download/SystemConsistency/SoftwareUpdate/SESU_latest_version/SESU_latest_setup_sfx.exe

(This will be an immediate download)

2) Run Windows Services.

3) Find "Schneider Electric FUS Service"

4) Right-click on it and choose "Stop"

5) Find "Schneider Electric SUT Service"

6) Right-click on it and choose "Stop"

7) Install the "SESU_latest_setup_sfx.exe" that you grabbed from Step 1.

8) Install the HMI License Manager update

9) Then install the HMI License Manager from the installer file once again.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre