How to Locate my PowerShelf unit?
Question:
How to Locate my PowerShelf unit?
Scenario:
APC by Schneider Electric recognizes that customers may need a quick and reliable way to physically identify a specific PowerShelf unit within a data center. This can be particularly useful when multiple PowerShelf units are installed across several racks or configured as part of a cascaded PowerShelf system.
Product Line:
SENVPS33KB2, SENVPS33KL-NP, SENVPS33KB3
Resolution:
The PMC indicator light can be used to help physically identify the PowerShelf associated with the PMC being accessed remotely.
This functionality can be controlled through the Redfish API:
Turn the indicator light ON
Method: PATCH
Resource: /redfish/v1/Managers/PMC_0
Action: Indicator light ON
After issuing the command, look for the PMC where the green and yellow LEDs are alternately flashing at 4 Hz. This identifies the physical PowerShelf associated with the PMC being accessed.
Resource: /redfish/v1/Managers/PMC_0
Action: Indicator Light OFF
If you have any clarifications, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.