How can we help you today?

What is the default IP address of the M172 Secure Interface Gateway when connected via USB?

Issue:

Default IP address of the M172 Secure Interface Gateway when connected via USB


Product Line:

M72


Resolution:

The default IP address after the connection of a PC to TM172 Secure Interface Gateway via USB mini-B connector is 192.168.254.254 .

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: