How can we help you today?

Why 277V for AI and High-Density Computing Infrastructure?

Question:
Why is 277V becoming increasingly relevant for AI, High Performance Computing (HPC), hyperscale, and other high-density computing environments?

Product Line:
APC by Schneider Electric power distribution solutions supporting applicable 277V and high-density computing environments – All applicable SKUs

Environment:
Global
Artificial Intelligence (AI), High Performance Computing (HPC), hyperscale, cloud computing, high-density IT, and next-generation data center environments.

Cause / Resolution:
Artificial Intelligence (AI), High Performance Computing (HPC), and cloud workloads are increasing the amount of power required by modern data center infrastructure. As compute density increases, delivering more power efficiently becomes increasingly important.

277V is becoming relevant to next-generation high-density infrastructure because a higher operating voltage can deliver the same amount of power with less current compared with lower-voltage alternatives such as 208V.

The progression can generally be viewed as:

• 120V – Legacy IT environments
• 208V – Modern enterprise IT environments
• 277V – High-density AI and hyperscale IT environments

More Power with Less Current

One of the fundamental advantages of higher voltage is that the same amount of power can be delivered using less electrical current.

For example, the reference material demonstrates an approximately 5 kW load:

• At 208V, approximately 24A is required.
• At 277V, approximately 18A is required.

Both examples represent approximately the same amount of delivered power, but the 277V example accomplishes this at lower current. Lower current can reduce stress on the supporting electrical infrastructure while allowing more power to be delivered efficiently to high-density IT equipment.

Reduced Electrical Losses

Electrical losses in conductors are influenced by current according to the relationship:

PLOSS = I² × R

Because the current component is squared, reductions in current can result in meaningful reductions in resistive losses when other conditions remain comparable.

This means that using a higher voltage to deliver a given amount of power can help reduce heat and energy losses within the electrical distribution path, allowing more usable power to reach the IT equipment.

Smaller Conductors and Supporting Infrastructure

Lower current requirements can also reduce demands on portions of the supporting electrical distribution infrastructure.

Depending on the electrical design and applicable requirements, lower current can contribute to the use of smaller conductors and cable sizes, smaller conduit and cable trays, and more efficient use of electrical distribution infrastructure.

This can become increasingly significant as data centers scale to support larger quantities of high-density computing equipment.
For illustration, assume the conductor path has the same resistance of 0.1Ω in both examples.

At 208V / 24A:
PLOSS = 24² × 0.1
PLOSS = 576 × 0.1
PLOSS = 57.6W

At 277V / 18A:
PLOSS = 18² × 0.1
PLOSS = 324 × 0.1
PLOSS = 32.4W

In this simplified example, reducing the current from 24A to 18A reduces the conductor loss from 57.6W to 32.4W, which is approximately a 44% reduction in resistive loss for the same assumed conductor resistance.

Supporting Higher Compute Density

The move toward AI is significantly increasing power density within the data center.

The reference material illustrates the progression in compute power requirements as:

• Traditional Enterprise: approximately 5–15 kW
• Modern AI: approximately 30–80 kW
• Future AI: 100+ kW

As these power requirements increase, the ability to distribute larger amounts of power while limiting current becomes increasingly valuable. 277V helps enable the higher power densities required by modern AI and HPC infrastructure.

In simple terms, 208V helps power modern servers, while 277V helps address the increasing power requirements of modern AI clusters.

Power Supply Efficiency

Many modern server power supplies are optimized for operation at higher input voltages. Where supported by the equipment design, higher-voltage operation can provide improved power conversion efficiency.

Improved conversion efficiency can contribute to:

• Reduced energy losses
• Reduced heat generation
• More efficient power delivery
• Lower operating costs
• Improved overall data center efficiency

These benefits become increasingly important as the number and power density of computing systems increase.

Built for the Next Generation of Computing

AI and HPC workloads are rapidly increasing the amount of electrical power required by compute infrastructure. The transition toward 277V reflects the need for electrical infrastructure capable of supporting increasing compute density efficiently and at scale.

The benefit of 277V is therefore not the higher voltage alone. The broader advantage comes from the ability to deliver greater amounts of power at lower current, reduce electrical losses, support increasingly dense compute environments, and improve the efficiency of the supporting power infrastructure.

APC by Schneider Electric Power Distribution Offerings

APC by Schneider Electric has power distribution offerings designed to accommodate the evolving electrical requirements associated with modern enterprise IT, AI, HPC, hyperscale, and other high-density computing environments.

The availability of higher-voltage power distribution options helps support the transition from traditional enterprise infrastructure toward increasingly power-dense AI infrastructure while addressing requirements for efficient and scalable power delivery.

Key Takeaway:

277V is becoming increasingly relevant because modern AI infrastructure requires significantly more power than traditional IT environments. Delivering that power at a higher voltage reduces the current required for the same amount of power.

This can provide several infrastructure advantages, including reduced electrical losses, more efficient use of conductors and supporting infrastructure, improved power delivery efficiency, and the ability to support higher-density computing environments.

The transition to 277V is therefore not simply about increasing voltage. It is about enabling higher-density compute, greater electrical efficiency, and infrastructure capable of supporting the next generation of AI and HPC workloads.


If you have any clarifications, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.

Schneider Electric Nigeria