How can we help you today?

What Contacts Are Needed for a HAND-OFF-AUTO Selector Switch?

What you need to know

For a standard HAND-OFF-AUTO (HOA) arrangement using a Schneider Electric Harmony 9001KS43 or 9001SKS43 3-position selector switch, use a 9001KA1 contact block.

With the C cam configuration:

  • HAND (left): NC contact closed
  • OFF (center): NO contacts closed
  • AUTO (right): NO contact closed

This provides two independent contact functions for the traditional HAND/OFF/AUTO control arrangement.

9001 selector switch contact organisation for HAND-OFF-AUTO function

HAND-OFF-AUTO selector switch configuration

The 9001KS43 is a Harmony 9001K 30 mm, 3-position, maintained selector switch head supplied without a contact block. Schneider Electric identifies it as compatible with the 9001KA1 contact block.

For standard HOA arrangement:

  • Use a 9001KA1 contact block.
  • The selector switch uses a C cam.
  • The left position corresponds to HAND.
  • The center position corresponds to OFF.
  • The right position corresponds to AUTO.

Contact operation by selector position

Selector positionOperating modeNC contactNO contact
LeftHANDClosedOpen
CenterOFFOpenOpen
RightAUTOOpenClosed

This arrangement ensures that HAND and AUTO are independent operating selections, while neither contact is closed in the OFF position.

Schneider Electric references

FunctionSchneider Electric referenceProduct description
Selector switch head9001KS43Harmony 9001K metal selector switch head, 30 mm, 3 positions, maintained/stay-put, supplied without contact block.
Selector switch head9001SKS43Harmony 9001SK selector switch referenced for the equivalent HAND/OFF/AUTO arrangement in the source FAQ.
Contact block9001KA1Contact block used with the C-cam selector switch to achieve the traditional HAND/OFF/AUTO contact arrangement. The Harmony 9001K documentation identifies 9001KA1 as a compatible contact block for these selector-switch configurations.

Launch Product Selector on se.com to configure a 9001selector switch according to your requirements or contact Schneider Electric Technical Support to check a configuration against your control scheme.

Schneider Electric Nigeria