How can we help you today?

ION Setup - "Network configuration seems corrupted" error

Issue

After logging into ION Setup, the following error messaged is displayed: "Network configuration seems corrupted. Do you wish to load the backup copy?"

Network configuration seems corrupted

Product Line

ION Setup

Cause

Due to a previous crash, interruption, or unsuccessful save, the network configuration files can sometimes become corrupted.

Resolution 1

Click Yes to see if it successfully loads the network configuration.

Resolution 2

If there is access to an existing Power Monitoring Expert (PME) 2020 or later installation, refer to this article to import the device list from PME.

Resolution 3

Try looking for manual backups of the network configuration files:

  • In File Explorer, go to View > check Hidden Items:

Hidden Items

  • Look for renamed copies of DEVINFO.DAT, IONSETUP.DAT, and SITEINFO.DAT. There may be some present in manually created folders in the C:\ProgramData\Schneider Electric\ION Setup folder or in other folders/drives. To restore:
    • Close ION Setup.
    • Move the files to the C:\ProgramData\Schneider Electric\ION Setup folder.
    • Rename the files to DEVINFO.DAT, IONSETUP.DAT, and SITEINFO.DAT respectively.

Resolution 4

Manually recreate the device network. To facilitate this:

  1. Manually add one device of each type, and at least one Ethernet site and one Ethernet Gateway site (if applicable). Refer to this article for the steps to add a device.
  2. Open File > Export Network.
  3. Open the exported .csv using Excel.
  4. Use Excel to populate the list with remaining devices and/or sites, following the formatting of the exported .csv.
  5. Save the .csv and close Excel.
  6. In ION Setup, open File > Import Network.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: