Actassi - cable support - set of 1 - 1U
NSYSPBOPB
Discontinued on: 30 Jun 2024
- What does the end of commercialization mean ?
End of commercialization is the last date Schneider Electric will accept an offer for this reference. However, after Sales Services (repair, spare parts, etc.) will continue until its end of life.
- Need more help
Contact Customer Care Center - available 24 a day.
NSYSPBOPB has not been replaced. Please contact your customer care centre for more information.
Allows to helps securing and guide the cables on the back of the enclosure
Fixed to the rear of the enclosure to support and fix the cables
Height adjustable with a step of 44.45 mm (1U)
Material: zinc-coated steel
29,069.32 NGN