Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How reliable is the KNX system ?

Article available in these languages: Dutch

The KNX system is for decades worldwide a proven conceptand installed in more then 100.000 residential and commercial buidlings.
The simple system platform works fail-safe.
A central unit is not necessary, the intelligence is within the components itself. Removal of one component keeps the system fully in function.
By means of a back-up battery operational functionallity is guaranteed, even even when supply power is down.

Schneider Electric Netherlands