Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the alternative for shockproof contactors LC1D*G10** ?

Article available in these languages: Dutch

An alternative for the shockproof contactors LC1DFG10** ( AC3: 12A ) and LC1DLG10*7 (AC3: 25A ) are contactors from
the TeSys D – range LC1D09*D up to LC1D38*D ( with DC control voltage ! ).

If the application has AC  control voltage, a rectifier bridge LAD4S123 is necessary.
The LAD4S123 is a rectifier block for mounting on top of the TeSys D contactor,
the control voltage is limited to 250VAC.

AC voltage is applied at the input and the DC voltage from a 4 diode bridge rectifier appears at the output.
It is intended only for small contactors.

LAD4S123

For your information:  DC output voltage from LAD4S123 is 0.9 * AC input voltage.
For example if you supply 230VAC / 50 or 60Hz, then the DC output voltage will be 207VDC.

Old shockproof values LC1D*G AC : 12g / 50ms, 15g / 11ms, 30g / 6ms, 50g / 6ms in all axes

The shockproof values  LC1D09 - D38*D are 15g /  11ms in all axes.

Schneider Electric Netherlands