Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Micrologic X - What is the usage of VPS (Voltage Power Supply) module ?

Article available in these languages: Dutch

Micrologic X is a self-powered protection control unit. The functions of protection do not require any power supply.
Below 20 % of the rated current a 24VDC external supply or the VPS module is needed to ensure the proper operation
and all the specified performances of Micrologic X for the measurement, diagnosis, display and communication functions.

Three important things to remember :
1) Basic protection is independent of this VPS module
2) During a trip event, this module is not able to provide power to the Micrologic X control unit
(due to the fact that the power is coming downstream the circuit breaker)
3) This module is a compulsory option when Micrologic 7.0 X is required

Schneider Electric Netherlands