Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is SF6 gas?

Article available in these languages: Dutch

SF6 is an artificial gas that has been widely used for decades in high and medium voltage electrical equipment, such as switchgear, as an insulating and arc quenching agent. The gas owes its popularity to its insulating and circuit-breaking properties, thermal capacity and stability. It is also inert, non-flammable and completely non-toxic in its pure form. SF6's highly insulating property allows it to significantly reduce the size of switchgear, crucial for many tight spaces.

Read more on SF6 and medium-voltage (Dutch) -->

Schneider Electric Netherlands