Search FAQs
Osisense XX - CSA certificate of the XX or VM ultrasonic sensors
The XX or Vm ultrasonic sensors are not CSA marked. They are cULus listed by the UL, and this mark appears in the product label. If a product is cULus listed, it means that UL tested the product to meet all the requirements under Canadian and US standards. Anything that has cULus mark can be used both in Canada and US. Attached corresponding certificate NRKH7.E480783, title Proximity Switches Certified for Canada, concerning all our ultrasonic sensors
Released for:Schneider Electric Philippines
Attachment(s)
Explore more
Explore more