Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How Current or Voltage Unbalance is calculated in Power Logic and ION...

Issue The formula that calculates the percent Current or Voltage Unbalance in Power Logic and ION meters has not been mentioned in Manuals. Product Line Power Logic and ION meters that are in...

What are S1, S2,and S3 in the LH4N2 wiring diagram?

Issue: S1, S2 and S3 buttons wiring diagram indication in LH4N2. Product Line: LH4N Environment: All Cause: Control wiring circuit Resolution: The S1, S2, and S3 are switch designations in the...

How to Download Marine Certificate for Compact NSX from SE Website

You can download the Compact NSX marine certificate via SE website by following the instructions below: 1) Go to your local SE Website: Singapore: se.com/sg Philippines: se.com/ph Malaysia: se.com/my...

Ways to format an APC by Schneider Electric Network Management Card (NMC 2...

Issue: What are the ways to format or reset an APC by Schneider Electric Network Management Card (NMC) back to defaults or factory settings? Product Line: NMC2 and NMC3 (AP9630, 31, 35 - AP9640, 41,...

PowerChute Network Shutdown v5 reports "Could not connect to Host over the...

Issue: PowerChute Network Shutdown v5 reports "Could not connect to Host over the network." when configuring with VMware ESXi 8 host. Product: PowerChute Network Shutdown version 5...

What is the difference between rigid and flexible cable on Acti9 iC60,...

Flexible vs. Rigid Wires: The Key Differences. Comparing Flexible vs. Rigid wire involves exploring the advantages and disadvantages of the two very different types of wire. A comparison narrows down...

How do I upgrade the firmware on an APC Network Management Card (NMC) or...

Issue You wish to upgrade your Network Management Card's (NMC) firmware or have been instructed to. You have a device such as a Smart-UPS, Smart-UPS Ultra, Easy UPS On-Line, Easy UPS 3-Phase,...

Wiring of RS485 Communications Networks

Issue This document attempts to explain correct methods of wiring RS485 communication networks in industrial environments based on various application notes and technical articles. Environment RS485...

Show more
Popular Video FAQsPopular Videos
Show more
Learn more through our Generic Knowledge FAQsGeneral Knowledge
What is the difference between in-sync and in-phase?

There is often confusion between the in-phase and the In-sync features of ASCO transfer switches. It is important to understand the difference between these features especially during the process of...

What is the selection criterion of Circuit Breakers for the Capacitor bank...

The selection should be done after derating the Circuit Breaker taking into consideration voltage variation and capacitors tolerances that could increase nominal current up to 1.5In. The Derating...