Philippines
Welcome to the Schneider Electric Website

Welcome to our website.

You can choose another country to view available products or go to our Global website for company information.

Choose another country or region
  • Default Alternative Text

    Solutions for OSHA and NFPA 70E Compliance

  • Read

    • Read more about Schneider Electric solutions

      Brochure: Compliance Solutions for NFPA 70E

      This brochure provides an overview of the steps facilities can take to meet the requirements of NFPA 70E. It also includes information for strategies to mitigate the potential for an arc flash event. Read more: Compliance Solutions for NFPA 70E
    • Read more about Schneider Electric solutions

      Handout: Electrical Safe Work Practices Policy

      The Electrical Safe Work Practices policy establishes responsibilities and defines procedures to properly protect the workers.
    • Read more about Schneider Electric solutions

      Brochure: Switchgear "Virtual Main" Arc Flash Mitigation System

      Low-voltage switchgear and switchboards can be subjected to dangerous levels of arc flash incident energy when fed directly from a power transformer. The addition of a virtual main system reduces the arc flash energy on the entire low-voltage switchgear, including the main incoming section. Other solutions do not protect the entire lineup. Read more: Switchgear "Virtual Main" Arc Flash Mitigation System
    • Read more about Schneider Electric solutions

      Brochure: Engineered Solutions For Infrared Scanning Applications.

      Make infrared inspections without disturbing operations and comply with NFPA 70E requirements. Read More
    • Read more about Schneider Electric solutions

      Handout: Remote Racking System

      Remote racking systems (RRS) allow circuit breaker racking operations to be performed via a control panel located away from the cell, which removes the operator from manual contact with the circuit breaker. Read more: Remote Racking System
  • Learn

    White Paper: Arc Flash Labels - A Sticky Situation


    This white paper focuses on the new labeling requirements resulting from recent revisions to the NFPA 70E and NEC standards. It will also discuss some ‘sticky’ situations relative to labeling, as well as best practices and considerations for arc flash labels. Learn more: Arc Flash Labels - A Sticky Situation

    White Paper: Roadmap to Compliance with NFPA 70E


    There are five important steps that companies should take to reduce the occurrence of electrical accidents.These steps are required as part of The National Fire Protection Association (NFPA) standard 70E®, which provides a detailed reference for facilities to meet the requirements of electrical workplace safety. A sixth step assists the facility owners with fine-tuning the electrical system for safety and operability. Learn more: Roadmap to Compliance with NFPA 70E

    White Paper: Mitigating Arc Flash Hazards


    This paper will address Engineering Controls to reduce the degree of hazard and/or risk associated with an arc flash event. The engineering controls covered will either: 1) Reduce arc flash energy to a level where permitted tasks can be performed, or 2) Locate the worker so that he/she is not subject to harm. Learn more: Mitigating Arc Flash Hazards

    White Paper: Arc Flash Analysis - IEEE Method versus the NFPA 70E Tables


    This paper discusses the basic differences between the IEEE 1584 method and the NFPA 70E task tables. A recommended specification is also provided for facility owners who are interested in achieving compliance with the regulations.

The Chat is available now