{}

Våra varumärken

Impact-Company-Logo-English Black-01-177x54

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
Hur kan vi hjälpa dig idag?
How to configure RemoteConnect x70 Device as Modbus RTU Slave?
When the SCADAPack x70 device is operating as a Modbus RTU Slave, it can communicate with up to 4 Modbus RTU Masters, 1 through each serial port on the device.

Supported Data Types
When the SCADAPack x70 device is operating as a Modbus RTU Slave, it supports the IEC 61131-3 data types described below.
SCADAPack Object TypeModbus IEC TypeFunction CodeModbus Operation
DIGITALDISCRETE1Read Coils
2Read Status Registers
5Write Coil
15Write Multiple Coils
ANALOGUINT3Read Holding registers
4Read Input registers
6Preset Single Register
16Preset Multiple Registers
DINT3Read Holding register pairs
4Read Input register pairs
16Preset Multiple Register pairs
INT3Read Holding registers
4Read Input registers
6Preset Single Register
16Preset Multiple Registers
REAL3Read Holding register pairs
4Read Input register pairs
16Preset Multiple Register pairs
DISCRETE1Real Coils (up to 16)
2Read Input Status (up to 16)
15Write Multiple Coils (up to 16)
COUNTERUINT3Read Holding registers
4Read Input registers
6Preset Single Register
16Preset Multiple Registers
UDINT3Read Holding register pairs
4Read Input register pairs
16Preset Multiple Register pairs

To configure RemoteConnect Project as Modbus RTU Slave:
1. Verify that Modbus RTU Slave checkbox is checked from Project Configuration Options



2. Go to Configuration Modbus >Slave/Server to Select Modbus Slave Addressing Mode
at least one of the serial ports needs to be configured for Modbus


  • Port Function Should be ‘Modbus’
  • Port Mode, Baud rate and the Parity should be configured as the Modbus Master
  • Modbus RTU Slave >Station Address should be unique per Modbus Link between 1 to 247
3. Go to Configuration Modbus >Slave/Server to Select Modbus Slave Addressing Mode



SCADAPack x70 devices support 5-digit and 6-digit Modbus addressing, you can set up a Modbus Slave to have any of these registers available to a Modbus Master that requests them.

The table below maps 5-digit Modbus address ranges to the equivalent 6-digit Modbus address range.
Use this information to stay within the appropriate address range when moving from 5-digit to 6-digit Modbus addressing.
Type5-Digit Modbus Address RangeEquivalent 6-Digit Modbus Address Range
Coil1 to 99991 to 9999
Status register10001 to 19999100001 to 109999
Input register30001 to 39999300001 to 309999
Holding register40001 to 49999400001 to 409999

4.  To assign a Modbus address to an Objects, Open Objects >Object Configuration
Select and object and from Modbus tab insert the proper Modbus address and type


5. Apply and save the project










Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj