Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
Where can I find Altivar ATV12 and Altivar ATV32 firmware update instructions?
Issue:
ATV12 and ATV32 firmware update instructions.

Product Line:
Altivar ATV12 and ATV32

Environment:
All

Cause:
Needs to get the instructions on how to update the firmware on the ATV12 and ATV32 drives.

Resolution:
To update the ATV12 or the ATV32 firmware revision you will need a VW3A8121 Multiloader and a VW3A8122 cable.
and see the attached file for instructions.

Schneider Electric Slovakia

Príloha(-y)
Multiloader_firmware_update_V2.pdf [1.28 MB]