Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
Can I read simple ASCII characters into my Quantum PLC via a Network Option Ethernet module (140NOEXXXXX)?

Goals and Symptoms:

Can I read simple ASCII characters into my Quantum PLC via a Network Option Ethernet module (140NOEXXXXX)?

Causes and Fixes:

No. The quantum Network Option Ethernet modules (140NOEXXXXX) can only accept Modbus TCP/IP messaging. They cannot read in ASCII characters. ASCII messaging can be accomplished either via the 140ESI06210 ASCII interface module or via the XMIT (984LL) or XXMIT(IEC) instruction from Modbus port #1 on the CPU module.