Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
Why is command switching not visible on the ATV71?
Issue:
Command switching is not visible on the ATV71.

Product Line:
Altivar 61, Altivar 71

Environment:
All serial numbers, all model numbers

Cause:
N/A

Resolution:
On the ATV61 or the ATV71, command switching will not be visible if profile is "not separate".   Profile set to "not separate" means the command comes from the same place as the reference.