Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
How Unity Pro application can be restored from SD memory card to a CPU?
A Unity Pro application can be restored from SD memory card to Modicon PLC CPU like M580 and M340.

1- Switch off the PLC
2- Insert the SDCard "where the application saved in" into the CPU
3- Switch on the PLC
Let the PLC for few moments till the application is being transferred to the CPU.