Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Functions and characteristics : UA controller
The UA controller is used to create a sourcechangeover system integrating the following automatic functions:
1) transfer from one source to another depending on the presence of voltage UN on the “Normal” source
2) startup of an engine generator set
3) shedding and reconnection of non-priority circuits
4) transfer to the “Replacement” source if one of the phases on the “Normal” source fails. The UA controller can control Compact NS, Compact NSX and Masterpact NT/NW devices.

Functions and characteristics : UA controller

Schneider Electric Thailand

Attachment(s)
UA Controller.pdf [496.75 KB]