{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please check the box"}}}
Search FAQs

What control circuit voltage is needed for the ATS48?

Issue:
What control circuit voltage is needed for the ATS48?

Product Line:
Altistart 48

Environment:
All

Cause:
Installation

Resolution:

For ATS48...Q the control circuit voltage is 220 - 15 % to 415 + 10 %, 50 / 60 Hz & ATS48..Y control circuit voltage is 110 - 15 % to 230 + 10 %, 50 / 60 Hz as indicated in the attached chart. This is AC voltage. 

Control voltage should be applied to the CL1 & CL2 terminals.