Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are Diagnostic Codes on Power Meter PM3200 series means ?

If the combination of the backlight and the error / alert icon indicates an error or an abnormal situation, navigate to the diagnostics screen and find the diagnostics code.

current perface

You can follow the instruction and Possible solutions as the table below.
Diagnostic
Code
PM3200PM3210PM3250PM3255DescriptionPossible Solution
-////LCD display is not visible.Check and adjust LCD contrast/backlight
settings
-////Push buttons do not function.Restart the power meter by power off and power on again.
101, 102////Metering stops due to internal error.
Total energy consumption is displayed.
Enter the Configuration mode and implement Reset Config.
201////Metering continues.
Mismatch between frequency settings and frequency measurements
Correct frequency settings according to the nominal frequency of the network.
202////Metering continues.
Mismatch between wiring settings and wiring inputs.
Correct wiring settings according to wiring inputs.
203////Metering continues.
Phase sequence reverses.
Check wire connections or correct wiring settings.
205////Metering continues.
Date and time have been reset due to loss of power.
Set Date and Time.
206-/-/Metering continues.
Pulse is missing due to overload on energy pulse output.
Check the energy pulse output settings and correct if needed.
207////Metering continues.
Abnormal internal clock function.
Restart the power meter by power off and power on again.

Schneider Electric Thailand

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center