Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ATV310 - setting command run via Keypad and adjust speed by analog input 4-20mA


Setting command run via Keypad and adjust speed by analog input 4-20mA.

1. Go to Conf ---> FULL

- program 401 (Reference channel 1)  to 01 (Analog terminal)
- program 407 (Command channel 1)  to 03 (Remote display)
- program 406   to   02 (Separate)
2. Scaling the analog input signal
- program 204-  to   0A ( 0A is Current: x-y mA)
- program 204.1  (AI1 current scaling parameter of 0% * (0-20mA))
- program 204.2  (AI1 current scaling parameter of 100%  * (0-20mA))

Schneider Electric Thailand