How can I introduce a control character "carriage return" in a String? String = "message"+ CR (carriage return)

Goals and Symptoms

How can I introduce a control character "carriage return" in a String?

String = "message"+ CR (carriage return)

Facts and Changes

Vijéo-Designer V4.2

Causes and Fixes

In Java, the "carriage return" character is "\n". So, to insert a carriage return into a string, use this character in a string concatenation expression.
The file name is: "carriage return.zip".
The script action inside the switch, You will see the syntax for string concatenation and how the carriage return character is used.
carriage return.zip

ชไนเดอร์ อิเล็คทริค Thailand

ดูข้อมูลเพิ่มเติม
รุ่น:
บทความที่อาจช่วยได้
ดูข้อมูลเพิ่มเติม
รุ่น: