Schneider Electric Unveils TeSys Deca Advanced: The Future of Motor Management
Chicago, IL, USA
17/03/2025
- Schneider Electric introduces the TeSys Deca Advanced contactor at ProMat 2025, setting a new standard in energy efficiency, reliability, and operational simplicity
- The TeSys Deca Advanced enhances motor control performance, significantly reducing operational costs while promoting sustainability
- Its innovative design features a streamlined wiring system and advanced digital capabilities, all while supporting high-efficiency motors
Schneider Electric, a global leader in digital transformation for energy management and automation, announced the launch of TeSys Deca Advanced, a contactor solution designed to revolutionize motor management in the era of Industry 4.0, today at ProMat 2025 in Chicago.
Designed with a streamlined wiring system and advanced digital capabilities for a range of industrial applications, the TeSys Deca Advanced stands out with its wide-band coil technology, capable of accepting control voltage inputs from 24V to 500V AC/DC. This innovative feature not only withstands voltage fluctuations but also minimizes energy consumption, resulting in reduced CO2 emissions and operational costs.
“Innovation is essential in the design of material handling, packaging, and logistics machinery as OEMs strive to meet the rapidly changing demands of this expanding industry," said Antonio Di Vaira, SVP of Power Products NAM Hub at Schneider Electric. "With the new TeSys Deca Advanced, we're excited to help machine builders optimize their solutions, reducing space and energy requirements. It's all about pairing advanced digital capabilities with operational simplicity, making their work easier and more efficient.”
TeSys Deca Advanced simplifies installation and maintenance processes. Its ergonomic three-layer setup organizes wiring for optimal visibility and accessibility, making maintenance and troubleshooting easier and more convenient. With one-click connection technology, installation efforts are reduced by up to 75%, allowing for rapid deployment in critical environments where uptime is essential. Additionally, the wide-band coil technology reduces complexity in selection and inventory management, facilitating smoother operations.
TeSys Deca Advanced is engineered for reliability, having undergone rigorous testing to ensure optimal performance. Its robust 100 kA short-circuit current rating with circuit breakers provides much needed flexibility for machine builders in their designs. TeSys Deca Advanced is designed to enhance operational efficiency across various sectors, including manufacturing, HVAC, and industrial facilities. By integrating cutting-edge technology with a focus on innovation and sustainability, Schneider Electric continues its commitment to maximizing uptime and delivering exceptional value.
To learn more about TeSys Deca Advanced, or to speak with a product expert, please visit the Schneider Electric booth #S659 at ProMat 2025, March 17-20, 2025, in Chicago.
Contact press

Thomas Eck
Media Relations Manager917-797-4974 thomas.eck@se.com
Adoption of Wiztrust's Blockchain Certification Platform
From October 2nd, 2019, in order to secure its communication, Schneider Electric certifies its contents on Wiztrust. You can check the authenticity on the website Wiztrust.com for Corporate communications.