Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What are the perforation pattern percentages of the NetShelter SX, SV or VX cabinet?
Issue:
There is a request for the perforation pattern percentage information for NetShelter cabinets.

Product Line:
NetShelter SX, SV and VX

Environment:
All versions and serial ranges.

Cause:
Some equipment manufacturers may request minimum perforation pattern percentages for the front and rear doors of an enclosure which houses their equipment. The most updated specifications can always be found in the owners manual of the enclosures in question.

NOTE: the perforation pattern percent of the equipment itself should be at least as open as the equipment demands of the enclosure doors.

Resolution:
see attached file.
There is also information in the NetShelter SX Bid Specifications document on the APC website.

Schneider Electric Việt Nam

Phần đính kèm
20120402 NetShelter Perforation Percentages Defined Rev4.pdf [21.14 KB]
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi:

Bạn cần trợ giúp?

  • Công cụ chọn sản phẩm