Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How can I integrate my SMT Smart-UPS with third party applications?
Issue:

How can I integrate my SMT Smart-UPS with third party applications?

Product Line:

Smart-UPS SMT

Environment:

All models except for SMT1000RM1U and SMT1500RM1U, UPS Firmware Rev 9.0 or greater

Cause:

APC by Schneider Electric uses a proprietary protocol called Microlink to communicate with APC branded software solutions. This protocol is used by all SMC, SMT, SMX, and SURTD series Smart-UPS products. Some customers may want to integrate UPS communications directly with their own applications.

Resolution:

To allow for third party integration APC has enabled Modbus communications on all SMT series Smart-UPS (except for the SMT1000RM1U and SMT1500RM1U).
The UPS units must be running UPS firmware version 9.0 or greater.


Documentation for Modbus integration (and other Communications Information) is available via the following two App Notes:
AN-176 "Modbus Implementation in APC Smart-UPS"
AN-177 "Software interface for Switched Outlet and UPS Management in Smart-UPS"
AN-181 "Smart-UPS Communications"


You can find these and many other APC App Notes HERE.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi:

Bạn cần trợ giúp?

  • Công cụ chọn sản phẩm