Issue:
PowerChute reports it cannot connect to vCenter Server
Product Line:
PowerChute Network Shutdown version 4.x
NOTE: For PowerChute Network Shutdown version 5, see Schneider Electric FAA000265038 PowerChute Network Shutdown version 5 reports "Cannot connect to vCenter Server over the network."
Environment:
VMware vCenter Server versions 6.7 and 7.0
Cause:
The wrong port has been configured, or the port is blocked.
In the example above, port 9443 was entered. Port 9443 is the port used by vSphere web client but not by PowerChute client.
Solution:
PowerChute Network Shutdown by default utilizes ports 443 or 80 to establish communication between the PowerChute client and vCenter Server. Unless you have changed the default port assigned in vCenter Server, port 443 or 80 should be selected for communications.
See VMware knowledge base document "Required ports for vCenter Server 6.0 (2106283)"https://techdocs.broadcom.com/us/en/vmware-cis/vsphere/vsphere/6-5/vsphere-installation-and-setup-6-5/deploying-the-vcenter-server-appliance/vcenter-server-appliance-requirements/required-ports-for-vcenter-server.html#GUID-925370DD-E3D1-455B-81C7-CB28AAF20617-en
NOTE: With the release of PowerChute Network Shutdown 4.4.x You must select vCenter Server Protocol HTTPS, accept untrusted SSL certificates, or add the vCenter SSL certificate to the PowerChute keystore, and the port should be 443. HTTPS port 443 must be open on the local network and vCenter firewalls to allow for communications.
Other issues that will cause PowerChute not to connect are incorrect credentials entered or a firewall block.
For non-port-related issues, see the Troubleshooting section of the attached PowerChute VMware User's Guide.
Đã phát hành cho: Schneider Electric Việt Nam
Bạn cần trợ giúp?
Công cụ chọn sản phẩm
Nhanh chóng và dễ dàng tìm được sản phẩm và phụ kiện phù hợp cho các ứng dụng của bạn.
Nhận báo giá
Bắt đầu gửi yêu cầu bán hàng trực tuyến và chuyên gia sẽ liên hệ với bạn.
Nơi mua hàng?
Dễ dàng tìm nhà phân phối Schneider Electric gần bạn nhất.
Trung tâm Hỗ trợ
Tìm sự hỗ trợ cho mọi nhu cầu của bạn tại một nơi.