Issue:
Customer wants to run his ATV212 drive at 80 hz max.
Product Line:
ATV212
Environment:
Analog input scaling
Cause:
Using 0-10v input
Resolution:
Go to FH- set to 80, UL- set to 80.
Also need to adjust the scaling parameters:
For VIA - go to F201-0, F202-0, F203=100, F204-set to 80
For VIB - go to F210-0, F211-0, F212=100, F213-set to 80
Đã phát hành cho: Schneider Electric Việt Nam