Issue:
CCTV Adapter Pod Specifications
Product Line:
NetBotz
Environment:
NetBotz version 2/3/4 appliances
NBPD0123
Cause:
Pod specifications.
Resolution:
CCTV Adapter Pod 120
The CCTV Adapter Pod 120 works with the version 2 NetBotz 500 and NetBotz 420 as well as the version 3 400 and 500 series appliances
CCTV Adapter Pod Specifications
Product Line:
NetBotz
Environment:
NetBotz version 2/3/4 appliances
NBPD0123
Cause:
Pod specifications.
Resolution:
CCTV Adapter Pod 120
- Converts analog video source to digital
- The monitoring appliance can then utilize digital images for motion sensing, alert image captures, etc.
- CCTV Pod provides images up to 640x480 resolution, 24-bit color, and up to 30 fps
- Color & resolution may be limited by CCTV video source
- CCTV camera connects to either BNC, RCA, or S-Video input on CCTV Adapter Pod
- 1 CCTV camera per adapter pod
- NTSC, PAL, or SECAM video source input format
- Distance between Pod and WB500 base station can be extended with USB extension cables, or CAT5 or Fiber Pod Extenders
- External jacks for microphone (internal mike also), speaker, door switch sensor
The CCTV Adapter Pod 120 works with the version 2 NetBotz 500 and NetBotz 420 as well as the version 3 400 and 500 series appliances
Released for:Schneider Electric Global