Issue:
Does Schneider Electric offer a Modbus RTU to Modbus Ethernet TCP option on the ATS22 Soft Starter.
Product Line:
Altistart ATS22
Environment:
All
Cause:
Ethernet option on the ATS22 Soft Starter
Resolution:
The Soft Starter has a built-in Modbus port. A Modbus-to-Ethernet Gateway (EGX100SD) can be used to interface between Modbus and Ethernet communication.
Released for:Schneider Electric Global