Issue:
Looking for basic programming information for ATV32
Product Line:
Altivar ATV32
Environment:
All
Cause:
Programming configuration set up
Resolution:
CONF>FULL>SIM
bFr= Base motor frequency 60hz
nPr= HP of he motor
UnS= Rated motor voltage
nCr= Rated motor current (motor FLA)
FrS= Rated motor frequency
nSP= Ratd motor speed (rpm's on motor nameplate)
tFr= Max frequency
ItH= Motor thermal current (match motor FLA)
ACC= Acceleration (ramp up) time
dEC= Deceleration (ramp down) time
LSP= Low speed
HSP= High speed
Released for:Schneider Electric Global