undefined [object Object]
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Data Center Expert | How do hardware and software support contracts work?

Issue:
Details on how extended hardware warranty and software support contracts work for StruxureWare Data Center Expert.

Product Line:
StruxureWare Data Center Expert (DCE)
- Basic Appliance (AP9465)
- Standard Appliance (AP9470)
- Enterprise Appliance (AP9475)
- Virtual Appliance (AP94VMACT)
StruxureWare Central (SWC)
InfraStruXure Central (ISXC)

Environment:
StruxureWare Data Center Expert (all versions)
StruxureWare Central (all versions)
InfraStruXure Central (all versions)
Software Support Contract

Cause:
StruxureWare Data Center Expert appliances come with 2 years of factory hardware warranty and no software support.  The Data Center Expert appliance and any additional device packs must be under active and complete software support in order to receive technical support and software upgrades.  Software support contracts are required for the server which has a default 25 nodes (covered under base software support SKUs) as well as each additional node license. Modbus license keys and surveillance keys do not currently require support contracts.

Resolution:

Hardware Support Contracts

StruxureWare Data Center Expert Appliances can have hardware warranty up to a total of 5 years, which includes 2 years of factory warranty. Hardware support must be continuous for the duration of coverage without lapse. Factory warranty details and hardware extension SKUs are provided below:

Model ApplianceYear 1Year 2Year 3Year 4Year 5Year 6
AP9465FactoryFactoryWMS1YRHWBASIC-DIGIWMS1YRHWBASIC-DIGIWMS1YRHWBASIC-DIGIOut of HW Support
AP9470FactoryFactoryWMS1YRHWSTD-DIGIWMS1YRHWSTD-DIGIWMS1YRHWSTD-DIGIOut of HW Support
AP9475FactoryFactoryWMS1YRHWENT-DIGIWMS1YRHWENT-DIGIWMS1YRHWENT-DIGIOut of HW Support


Extended Hardware Warranty Statement of Work: https://download.schneider-electric.com/files?p_Doc_Ref=SPD_RJEN-7G4G48_EN


Software Support Contracts

There is limited help that can be provided for trial installation of the Virtual Appliance (AP94VMTRL).  Software support can not be purchased for a virtual appliance until it is activated using a virtual machine activation key (AP94VMACT).  Contact your local sales representative for purchase related questions.

Support contracts start at the date of purchase or are appended to the end date of previous contracts. In the case of a Schneider Electric installation/configuration service of the systems, the support will begin when the configuration is completed.  Please note that should your software support contracts lapse, you can put your server and license keys back under support, but backdating to the end of the previous support contracts will be required.

The updated software statement of work can be found on the Data Center Expert product page under Documents here.


Determining the amount of Device Nodes Installed

NOTE: Technical support utilizes the EcoStruxure IT Entitlements portal at https://ecostruxure-it-entitlements.se.com to determine the number of install licenses.  Installed licenses and DCIM Assets may not match if licenses have been redeemed against the server in the EcoStruxure IT Entitlements portal but not yet added into the software for use.

1) Open the Data Center Expert Desktop Client.  Instructions on installing can be found within the knowledge base Video: Data Center Expert | Desktop Client Requirements, Download, & Installation.

2) Log in using administrator credentials.

3) System menu > Server Administration Settings > License Keys.

4) Add all of the Node Count (column) values that have a License Type (column) of StruxureWare Data Center Expert Device Pack.


Determining Software Support SKUs Needed

1) A Base software support contract is always needed and covers the base 25 nodes installed on the appliance.  This SKU is different depending on the model appliance.  For help determining an appliance model, see knowledge base Data Center Expert | Location of the Model, Serial Number, and MAC address .

Model1 Year Software Support SKU3 Year Software Support SKU
AP9465WMS1YRBASIC-DIGIWMS3YRBASIC-DIGI
AP9470WMS1YRSTD-DIGI WMS3YRSTD-DIGI
AP9475WMS1YRENT-DIGIWMS3YRENT-DIGI
AP94VMACTWMS1YROVM-DIGIWMS3YROVM-DIGI


3) Take the node count determined above in step 4 of Determining the Amount of Device Nodes Installed and subtract 25 nodes from the total.  This is due to the base 25 nodes being covered under the base software support agreement outlined in the previous step.
NOTE: Different quantities of the SKUs below need to be purchases to provide enough software support to cover all of the licenses, in addition to the base software support as outlined above.  If there is an additional qty. 4 of 25 node device packs installed, a 100 node software support SKU can be purchased.  The total added up software support, must match the total added up installed device node packs.

License Count1 Year Software Support SKU3 Year Software Support SKU
25WMS1YR25N-DIGIWMS3YR25N-DIGI
100WMS1YR100N-DIGIWMS3YR100N-DIGI
500WMS1YR500N-DIGIWMS3YR500N-DIGI
1000WMS1YR1000N-DIGIWMS3YR1000N-DIGI

Software Support Example 1

Model AP9465 with a total of 25 device nodes installed.
Software Support Needed: Base + 0 nodes.

Qty.1 Year SKU3 Year SKU
1WMS1YRBASIC-DIGIWMS3YRBASIC-DIGI

Software Support Example 2

Model AP9470, with a total of 250 device nodes installed.
Software Support Needed: Base + 225 nodes.

Qty.1 Year SKU3 Year SKU
1WMS1YRSTD-DIGIWMS3YRSTD-DIGI
1WMS1YR25N-DIGIWMS3YR25N-DIGI
2WMS1YR100N-DIGIWMS3YR100N-DIGI

Software Support Example 3

Model AP94VMACT, with a total of 1275 device nodes installed.
Software Support Needed: Base + 1250 nodes.

Qty.1 Year SKU3 Year SKU
1WMS1YROVM-DIGIWMS3YROVM-DIGI
2WMS1YR25N-DIGIWMS3YR25N-DIGI
2WMS1YR100N-DIGIWMS3YR100N-DIGI
1WMS1YR1000N-DIGIWMS3YR1000N-DIGI




Schneider Electric Global

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: