Issue
How to configure the EHC3020 for event counting.
Product Line
All versions of the Advantys Configuration Software.
Environment
Windows 7
Resolution
Wire the 'EHC3020' to the incremental encoder.
- Double click on the 'EHC3020' module to open the properties window for the module.
- Configure the parameters as shown.
- Start the PLC.
- Set the Input Validation bits to Off.
- Set the Counter Enable to On.
Released for:Schneider Electric Global