Issue:
The user would like to know if fuses are included with the meter when purchased
Product Line:
Energy Meter
Environment:
Protective Fuses
Resolution:
Fuse Packs/Fuses are not included with the Energy Meter.
The fuses are typically provided by the installer or can be purchased as an accessory called fuse packs.
The fuse packs come with 1/2 A SLO-BLO rating and can be ordered in packs of 1, 2, or 3.
Below are the part numbers for the fuse packs.
EMFP1 Energy Meter Fuse Pack, Set of 1 (includes 1 fuse)
EMFP2 Energy Meter Fuse Pack, Set of 2 (includes 2 fuses)
EMFP3 Energy Meter Fuse Pack, Set of 3 (includes 3 fuses)
Released for:Schneider Electric Global
Discontinued
Discontinued