undefined [object Object]
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the pin out for the M221 RS485 serial port?
Issue:
What are the pin outs for the M221 RS485 serial port?

Product line:
M221

Environment:
Ecostruxure Machine Expert Basic (formally SoMachine Basic).

Cause:
Issues with communication with the M221 serial port configured for RS485.

Resolution:
The pin out for the M221 RJ45 serial port is attached.

Schneider Electric Global

Attachment(s)
M221 RS485 serial port.docx [64.59 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.