Issue:
EPF2 fault on ATV32 or ATV320 when using Ethernet.
Product Line:
ATV32/ATV320
Environment:
All
Cause:
FDR detected fault
IP address duplication detected fault
Resolution:
First check the FDR on the Ethernet IP card is deactivated. In case the FDR is activated, that will explain the "EPF2" fault. The reason is that the Drive is waiting for a configuration from PLC, but PLC doesn't answer once the timeout is reached. This causes the drive to trip in "EPF2".
The second reason for "EPF2" fault is the range of IP address. In case of IP address 192.0.0.x and Sub net mask of 255.255.255.0 can cause "EPF2". Change the range of the IP address.
Additionally, an incorrect configuration of the drive can cause this fault when using Assemblies other than 100 and 101. Drive must be configured as follows:
EPF2 fault on ATV32 or ATV320 when using Ethernet.
Product Line:
ATV32/ATV320
Environment:
All
Cause:
FDR detected fault
IP address duplication detected fault
Resolution:
First check the FDR on the Ethernet IP card is deactivated. In case the FDR is activated, that will explain the "EPF2" fault. The reason is that the Drive is waiting for a configuration from PLC, but PLC doesn't answer once the timeout is reached. This causes the drive to trip in "EPF2".
The second reason for "EPF2" fault is the range of IP address. In case of IP address 192.0.0.x and Sub net mask of 255.255.255.0 can cause "EPF2". Change the range of the IP address.
Additionally, an incorrect configuration of the drive can cause this fault when using Assemblies other than 100 and 101. Drive must be configured as follows:
- Ref 1= Communications card
- Profile= Separate controls
- CMD switching= C312
- CMD channel 1= Communication card
- CMD channel 2= Terminal control
- Ref 2 Switching= C313
- Ref 2 Channel= AI1 or AI2
Released for:Schneider Electric Global