{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the maximum number of drives you can daisy chain using Modbus TCP/IP on an ATV32
Issue:
Maximum number of drives to daisy chain

Product Line:
ATV32, ATV61 and ATV71

Environment:
Modbus TCP/IP
Daisy chain part number
ATV32 - VW3A3616
ATV71 or ATV61 - VW3A3310D

Cause:
None

Resolution:
The maximum number of devices is 32.  However, there may be some limitations.  Please see the attached.

Schneider Electric Global

Attachment(s)
ATV in Ring or daisy chain topology.pdf [76.25 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: