undefined undefined
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: How do you set up Preset Speeds on the Altivar Process Drives?

Article available in these languages: Finnish, Japanese

Issue:
Preset Speeds set up on Altivar Process Drives.

Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
All serial numbers for the Altivar Process Drive

Resolution:



Preset speeds programming
Menu 5 complete settings enter
Menu 5.9 Generic Functions enter
Scroll down to Preset speeds
Assign preset speeds
DI2= Preset speed 2
DI3= Preset speed 4
DI4= Preset speed 8
DI5= Preset speed 16

0 0 0 0 Reference 1 ref 1 or Low speed
0 0 0 1 SP2
0 0 1 0 SP3
0 0 1 1 SP4
0 1 0 0 SP5
0 1 0 1 SP6
0 1 1 0 SP7
0 1 1 1 SP8
1 0 0 0 SP9
1 0 0 1 SP10
1 0 1 0 SP11
1 0 1 1 SP12
1 1 0 0 SP13
1 1 0 1 SP14
1 1 1 0 SP15
1 1 1 1 SP16

Example: Setting the low speed to 30 hz will be your 1st. preset speed.  This means that when only the run command (DI1) is enabled the drive should ramp up the motor to 30 hz.  if DI2 has been set to 2 preset speeds and preset speed 2 is set to 40 hz, then when DI1 and DI2 are enabled the drive will run the motor at the second preset speed.   if DI3 has been set to 4 preset speeds and preset speed 3 is set to 50 hz, then when DI1 and DI3 are enabled the drive will run the motor at the 3rd preset speed.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: