undefined [object Object]
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the recommended replacement for a TWDLCAA10DRF Twido controller?
Issue:
Is there a replacement for the Twido TWDLCAA10DRF?

Product line:
Twido, M221

Environment:
TwidoSoft, TwidoSuite, Ecostruxure Machine Expert Basic.

Cause:
Product obsolescence .

Resolution:
The recommended replacement for a TWDLCAA10DRF Twido controller is the TM221C16R controller or if you want Ethernet the TM221CE16R.

Characteristics Twido Reference vs Characteristics M221 Reference

Total I/O: 10 (Twido) vs 16 (M221)
Input: 6 (Twido) vs 9 (M221)
Relay Output: 4 (Twido) vs 7 (M221)
Trans Output: 0 (Twido) vs 0 (M221)
Analog Input: 0 (Twido) vs 2 (M221)
Power supply: 240VAC (Twido) vs 240VAC (M221)

Software Compatibility:
- Machine Expert Basic (previously called SoMachine Basic) software can convert a Twido application to a M221 (except functions like Asi & CanOpen not supported by the M221)

Mechanical Compatibility:
- Same Width 70 mm & same Depth (Height) 90mm
- The M221 Length is higher due to TB in 5.08 mm pitch vs TB in 3.81mm pitch on Twido
- M221 can support TM2 Digital & Analog IO module
- All module & accessory TWD*** are not supported by M221 in particular CanOpen, Asi, Serial Interface & display module.
- Twido + CanOpen Module = M241 CanOpen
- Twido + Asi Module = M221 Eth + Eth/Asi Gateway

Schneider Electric Global

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: