{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What Product Line Replaces the Altivar 312 and Altivar 32 drives?
Issue:
Replacement for the Altivar 312/32 drives.

Product Line:
Altivar 312, Altivar 32 and Altivar 320 Machine Drive (ATV312, ATV32, ATV320)

Environment:
All serial numbers for Altivar 312 and Altivar 320 Machine Drive

Cause:
N/A

Resolution:
The Altivar 312 and 32 drives are both smaller Constant Torque machine drives with mid-functionality features. The most current replacement would be the Altivar 320 Product line.  See attachments.

Altivar 312/32 to Altivar 320 Product Line
ATV320...C (IP20) replaces the ATV312 open style
ATV320...B (IP20) replaces the ATV32 open style

Altivar 312/32 vs Altivar 320 Product Line
The ATV320 has similar functionalities to the ATV312 and ATV32 but have a few minor differences to take into account when replacing.

Similarities and Differences

Size:
The ATV320...B (Book Shelf) is very similar in build and size to the ATV32 meanwhile the compact drives, ATV320...C, are built similar in size to the ATV312.

List of Other Differences
  • Programming layout is similar to that of the Altivar 32
  • All Altivar 320 drives have the Function Block capability
    • If drive shows "RDY" and will not start-up even if DI1 is on, then there may be a function block turned on
  • There are no LOCAL CONTROLS on the Altivar 320 drive.
    • No red STOP or green RUN buttons
  • New Safety Functions
  • Altivar 320 support numerous Communication Protocols such as Ethernet IP, DeviceNet, Modbus...
    • ATV320...C (Compact ONLY) requires the Communication Module (VW3A3600) when using a communication option card

See the Migration manual for additional details: https://www.se.com/us/en/download/document/QGH39563/

Schneider Electric Global

Attachment(s)
ATV312 Cross reference to ATV320.xlsx [128.66 KB]
Transition to ATV320 from ATV32.xlsx [136.67 KB]