undefined undefined
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
ATV32 / ATV320 Where is the ATV Logic functions programmed?

Article available in these languages: Spanish

Issue:
Programming ATV32/ATV320 Logic functions

Product line:
ATV32, ATV320, Altivar 32, Altivar 320, ATV Logic

Environment:
all

Cause:
n/a

Resolution:
Somove software is used to program the ATV Logic portion of the ATV32 and ATV320 drives. It cannot be done through keypad programming menus.  Once the ATV Logic program is complete, it is saved to the computer along with all other parameters as a .psx file.   This file can then be loaded to the VFD.

Schneider Electric Global

Attachment(s)
SoMove ATVLogicCapture.JPG.jpg [88.75 KB]
Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: