undefined [object Object]
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can you connect the Multi-loader to a VW3A1101 keypad to get the saved files?
Issue:
Can you connect the Multi-loader to a VW3A1101 to get the saved files?

Product line:
VW3A8121, VW3A1101

Environment:
all

Cause:
Manual for the Multi-loader shows you can connect the device to the VW3A1101 keypads.

Resolution:
The connection is shown for the purpose of flashing an update to the keypad firmware using the VW3A8121 Multi-Loader.
The program files that are stored on the VW3A1101 cannot be loaded to the Multi-Loader because the format is different.

Schneider Electric Global

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: