Issue:
Would like PowerChute Network Shutdown to begin the shutdown process once the UPS has run on battery for pre-determined amount of time.
Product Line:
PowerChute Network Shutdown
Environment:
All supported OS
Cause:
UPS on battery
Resolution:
- Log into PowerChute web interface by entering the systems IP address or FQDN on port 6547. Examples https://192.168.1.10:6547 or https://MYComputer@myOffice.com:6547
- Go to Configure Events
- Select UPS On Battery and click Shutdown
- Click Enable Shutdown
- Enter the desired amount of time you would like the UPS to run on battery prior to PowerChute starting the shutdown process and then click Apply.
For assistance installing PowerChute Network Shutdown see
How to install PowerChute Network Shutdown v5.1 onto Windows OS.
How to install, deploy, and configure PowerChute Network Shutdown version 5.x with VMware ESXi 7.x or above managed by vCenter Server 7.x or above.
Released for:Schneider Electric Global