undefined undefined
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the difference between LRD** and LR3D** relays?

Article available in these languages: Greek

LR3D** relays are used for the unbalanced loads : there can be different currents in the three phases of the overload relay ( according to its size ) . examples : distribution circuits which have not the same loads on each phases, or single phase motor. This relay will not trip if the currents in its phases are different.
The LRD** which is for balanced load : that means with the same current on the three phases ( e.g. a squirrel cage motor ).
This is the only difference between LRD & LR3D relay.

Schneider Electric Global

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: