{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is the ATV340 tested and approved for use on Single phase input to run 3 phase motors?

Article available in these languages: Spanish

Issue:
ATV340 on single phase input to run 3 phase motor
Product Line:
Altivar 340 - ATV340
Environment:
Single phase input power
Cause:
Customer does not have 3 phase power available.
Resolution:
No.
The ATV340 has not been tested or approved for use on single-phase power systems.
It requires 3-phase input power.
There are currently no plans to perform this testing.

It is possible to feed the DC Bus of the ATV340 drive so a front-end rectifier may be used.   Bonitron (http://www.bonitron.com/) has provided this type of device for years.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: