{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
There is a minimum firmware version for Unity Momentum processors at PV07 or greater.
Issue
Unity Momentum 171CBUx980x processors at a PV07 or greater require a minimum firmware version of 2.0.  PV07 processors cannot be downgraded to firmware versions less than 2.0.

Failure to follow these instructions may result in equipment damage.

It is recommended to upgrade to the latest firmware version.



Product Line
171CBUx980x - Unity Momentum Processors


Resolution
Unity Momentum 171CBUx980x processors at a PV06 or less can be upgraded or downgraded to any version without restriction.

Reference '171CBUx809x_Firmware History_SV2.01.pdf'


Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: