⚠ CAUTION ⚠ The information provided in this FAQ being considered as confidential content, as it can be exclusively used internally. This flag has been added automatically when the article is published with internal visibility only. |
ATV630ATV930 internal error 1 troubleshooting
Product Line:
ATV630 and ATV930 Process drives
Environment:
All
Cause:
• Unknown drive rating
• Power range or Voltage range parameter out of range
• Communication between CMP6 and Brick interrupted.
• Incompatible power brick in the system (voltage range / power range)
Resolution:
Unknown drive rating
Principle:
During initialization sequence, the compatibility of the different
device components is verified. If an component doesn't mach to the hardware configuration the fault InF1 occurs.
Probable causes
• Unknown drive rating
• Power range or Voltage range parameter out of range
• Communication between CMP6 and Brick interrupted.
• Incompatible power brick in the system (voltage range / power range)
Remedies
• Check the power rating and the voltage of the power bricks.
• connect to the SoMove service section and use the "drive type recovery function" to set a valid configuration to the power board.
• check the high speed link communication cables in the CMP6 and the CMI1
Released for:Schneider Electric Global