{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What do I do when I see "InstallShield Wizard: An error -5001 : 0x80070002 has occurred while running the setup" when installing Vijeo Designer 6.2 or associated Service Pack?

Article available in these languages: Spanish

Issue
When installing Vijeo Designer v6.2 or an associated Service Pack, the user encounters the message "InstallShield Wizard: An error -5001 : 0x80070002 has occurred while running the setup".

Product Line
Vijeo Designer 6.2

Environment
Windows 7, Windows 10

Cause
When InstallShield Wizard error "An error 5001 : 0x80070002 has occurred while running the setup" appears when installing Vijeo Designer 6.2 or associated Service Pack this means that there was an issue with the file when downloading the installation package and it may be incomplete or corrupted.

Resolution
If you redownload the installation file and this error message still occurs please contact Schneider Electric technical support to obtain a new download link.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Global

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: